Hi,
Having read the app report SBAA161–March 2009 Important Considerations to Assure a Safe POR, I've came up with a few questions.
In Specifications Related to POR section on page 2, it says:
The POR circuit of the TSC2007 contains a capacitor that is charged when the device powers up, and generates an internal reset signal when the voltage at the capacitor reaches a certain level.
What exactly is this "certain level"?
Also on the same page, it says:
tVDD_OFF time starts when TSC2007 VDD reaches 0V and remains at that level.
How much tolerance is to be expected around 0V? 10mV, 50mV, 100mV or whatever?
I'm asking these questions because sometimes I encounter this POR issue related to TSC2007. I believe the reason might be that when I connect a debugger to my board through a serial port, power supply pin of TSC2007 remain at about 120mV even though the board is not powered. And with this connection, sometimes it starts normally, sometimes not. But when I remove the debugger and power the board on, it always starts normally.
In addition, I must also admit that the power supply I use does not meet the VDD on/off ramp timings for TSC2007. I measured the ramp as 2kV/sec and spec says it must be 12kV/sec at least. But how critical is that actually? Because like I said, I never encountered any POR issue when trying without the debugger.
Thanks in advance.
Durmus