I am trying to use ad7846 using commands such as D8 and 98. The Y position is working ok ranging from 4 to 116. However, when i send 98 the X position is only ranging from 7 to 15 and also varies slightly with respect to Y position.
Top left (14,4) Top right(7,4)
Bot left(15,116) Bot right (9,112)
I am using the typical circuit from datasheet with the decoupling capacitors. The analog signals from X+ and Y+ behave similar to the digital data.