Other Parts Discussed in Thread: TSC2003, TSC2007
Hello
I have a TSC2017 touchpad (TSC2017EVM-PDK), connected to my computer on USB. I am trying to access it from my software using the visa library on python.
My problem is that the device seems to be undetected by the python/visa.
I run the following code to detect the devices connected to the computer:
import visa
rm = visa.ResourceManager("C:\windows\SysWOW64\visa32.dll")
rm.list_resources()
The last line returns an empty list, as if the connected device was not detected.
The device is connected properly to the computer - when I run the TSC2017EVM software, it detects the touch and shows it on screen.
I am using Windows 10 and running python 32-bit (to be compatible with the 32-bit visa.dll).
Any help would be great
Thanks,
Dror