Hello,
In this moment I am interesting to use the SPI Resistive Controller TSC2046E.
For use this controller I need some PCB layout information.
In the application report SLAA560 I have found the indication that "Connect the analog input pin AUX (or AUX IN, or IN), or V BAT to ground if not used."
It is correct connect this pin to ground through a capacitor 10uF 16V?
I want to use the internal TSC2046E voltage reference; It is correct connect also the V REF pin to ground with the same capacitor 10uF 16V?
Lastly if I not used the pen interrupt output (PENIRQ\) and the busy output (BUSY) Have I to connect them to ground or to the power supply? Can I use the same capacitor 10uF 16V?
Thank you very much in advance for your attention.
Best Regards