Dear Support team,
Our customer will use TSC2004 in their application.
Please answer some questions about the function of the PSM bit.
Q1:
Please tell me the delay time from when touch-on is detected until the PSM bit is set to 1.
Q2:
On the operation of the PSM bit during the Detecting Touch period after Preprocessing for Y Coordinate,
will the PSM bit be cleared to 0 during screen capacity precharge operation?
(Please refer to attached figure 40.)
Q3:
When touch-off occurs at the timing shown in Figure 40, will not the Z1 Coordinate and Z2 Coordinate process be executed?
After that, will the latest conversion data be read out for X-Data and Y-Data?
(Please refer to attached figure 40.)
Best Regards,
Hiroaki Masumoto