This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TPS82085: Package

Part Number: TPS82085

Hi,

We got a question from the customer about TPS82085.
Could you help us?

[Question]
They belive the package of this IC is uSiL which doesn't include the capacitor. But the features description in the datasheet describes it is Micro SiP. Which is correct?

Best Regards,
tateo

  • Hi Tateo,

    Yes this is a MicroSIL package as written in the "device information" table on the same page. Thanks for pointing this out, this will be corrected in the nest revision of the datasheet.

    _______________________________________________________________________________________

    TPS62825/6/7 – New High-density buck in 1.5x1.5QFN package! Also available in 2x1.5QFN, like TPS62823.

    5.5Vin, 2-3A buck with 4uA Iq and 1% accuracy. 4A sampling now!

  • In reply to Sabrina:

    Hi, Thank you for your reply. Please revise in the next revision of the datasheet.

    Best Regards,
    tateo

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.