This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

High efficiency 5v to 3.3V regulator (0.01mA-50mA)

Hello,

I'm desesperatly searching for the most efficient design to convert 5V to 3.3 V with a range from 0.01mA to 50mA.

The board is a atmega368P-Pu with some arduino arduino modules(sparkfun lis3Ddh accelerometer, and a micro slot both communicating in spi with the mcu)

The objectiv is to supply the system from a 5V power bank converted to 3.3 (because many modules use only 3.3V). Current consumptions are going from 0.01mA (sleep) to 50mA(LORA radio transmision).

First constraint is autonomy so is  power efficiency.

Thank for your help.

  • I tried to use webbench designer to determine the best design but i don't know how to specify a range of current consumption :)
  • Hi Gus,

    The TPS62740 should be best.

    Chris Glaser

    Texas Instruments

    ________________________________

    TPS62147 – New 17Vin, 2A buck with forced-PWM option for low output ripple.
    1% accuracy over temperature, 0.8V to 12Vout, pin-compatible to 4A (TPS62136), for industrial applications.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.