This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TPS62067: TPS62067

Genius 13210 points

Replies: 3

Views: 124

Part Number: TPS62067

Dear Sir,

We are required to design the voltage monitor mechanism that meets below illustration. Currently, the PGOOD signal is used for power sequence and also false detect. But for most of the application the minimum detection voltage will less than operation voltage range, thus violate the rule. For example, the TPS62067 has PGOOD falling threshold typ. 90%, not suitable for 5% tolerance application.

The question is:

For application with low voltage tolerance, (5%, for example) what will be the solution choice? Is there a power IC with high sensitive PGOOD signal or I should choose another power monitor IC?

For the standalone monitor IC, please help to give some suggestion. Please see below spec:

(a) 4 input, variable voltage detection range should include 1.2V~3.6V, tolerance target to +/- 1%.

(b)1 input, variable voltage detection range should include 3V~3.6V, tolerance target to +/- 2%.

Thanks, Ian.

  • Hello Ian,

    my pleasure to support you.

    I have some questions:

    -do you need to detect a DC voltage fall, or do you need also to detect AC events that fall outside the +-5% tolerance window?

    -Do you define this a fault because the 5% is the voltage tolerance of the load?

    -has your application heavy load transients?

    The internal PG of this device (and many other) are not built for a precise detection of load's input voltage tolerances, that's why the threshold is set to 90%, and the detection is relatively slow. Their purpose is rather to detect a general "no voltage" fault, or for sequencing purposes.

    If you need to be really strict on the voltage supervision, in terms of accuracy and bandwidth, I can't suggest anything but a voltage supervisor. TPS3702 is a good example. I would suggest you to open a dedicated post on the TPS3702, so that the right person for these kind of products will give you a deeper support.

    Thanks and best regards,

    Emmanuel

    All information in this correspondence and in any related correspondence is provided “as is” and “with all faults”, and is subject to TI’s Important Notice (http://www.ti.com/corp/docs/legal/important-notice.shtml).

    ____________________________________________________

    TPSM82480 - Industry’s smallest 5.5Vin, 6A DC-DC MODULE with forced-PWM and VSEL option.
    Ideal for FPGA and processor power. Only 3.6x7.9x1.55mm!  Order samples now!

  • In reply to Emmanuel Granatello:

    Dear Sir,

    Thanks for help.

    About your questions below:

    -do you need to detect a DC voltage fall, or do you need also to detect AC events that fall outside the +-5% tolerance window?

    [Customer] It should be able to detect both DC and AC events that fall outside the tolerance window.

    -Do you define this a fault because the 5% is the voltage tolerance of the load?

    [Customer] Yes. I just found I miss to attach the picture. Please see below, the monitor detection range should not overlap the normal power IC operational output range, but also has to within the load voltage range.

    For example, assume a DDR power rail may requires +/- 5% tolerance and a Power IC set to center with output +/- 2.5% tolerance. This leaves the monitor with maximum tolerance +/-1.25%. This is how I get the target tolerance for the monitor IC.

    -has your application heavy load transients?

    [Customer] Yes, heavy load transients may happen. They are for core power such as CPU and DDR.

     

    We would like to learn more about the voltage monitor. Customer might need to monitor 3~4 voltage rails with typical voltage(1.2V, 1.35V, 1.8V, 3,3V). We found TPS3702 is a good choice that no need to add external resistance. However it doesn’t support 1.35V rail monitoring and adding 3~5 monitor ICs also takes a lot PCB size. Do you think TPS386000 is a good choice?

    Thanks, Ian.

     

  • In reply to Ian Wang:

    Hello Ian,

    According to your answers, you really need a dedicated voltage monitor.

    To get any suggestion, please open a new post dedicated and tagging the TPS3702. You can ask your recommendation and an expert on that device will support you.

    If I answered the question related to the TPS62067, please give your feedback to this post.

    Thanks and best regards,

    Emmanuel

    All information in this correspondence and in any related correspondence is provided “as is” and “with all faults”, and is subject to TI’s Important Notice (http://www.ti.com/corp/docs/legal/important-notice.shtml).

    ____________________________________________________

    TPSM82480 - Industry’s smallest 5.5Vin, 6A DC-DC MODULE with forced-PWM and VSEL option.
    Ideal for FPGA and processor power. Only 3.6x7.9x1.55mm!  Order samples now!

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.