This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

BQ25606: BQ25606 can't into big current charger at 3V

Expert 2370 points

Replies: 11

Views: 553

Part Number: BQ25606

Hi,

Now we find BQ25606 can't into large current charger at Battery Volatge = 3V.

Then adjust VBAT to 3.4V and can into large current charger, why?

The below is BQ25606 schematic for your check again.

Thanks.

Best Regards,

Eric

 

  • In reply to Eric Chen4:

    I noticed there are input and output inductors. Can you remove them? The input inductor may cause startup failure due to voltage drop.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.