This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

LM5113: LMG1205 vs LM5113-Q1

Intellectual 665 points

Replies: 4

Views: 214

Part Number: LM5113

Hi,
we are looking for a replacement for LM5113 that is NRND. 
There is a LM5113-Q1 that from the datasheet looks almost identical as LM5113, has the same footprint
and pinout and it is active (not NRND).
What are the reasons that TI suggests LMG1205 as eplacement of LM5113, instead of LM5113-Q1 ?

Regards, Pawel

  • Hi Pawel,

    Please see this thread: e2e.ti.com/.../2331141

    Let me know if this doesn't answer your question. If it does, please press the green button for me!

    Best regards,

    Don Dapkus

    Gate Driver Applications Engineering Manager

    Dallas, TX USA

  • In reply to Don Dapkus:

    Hi Don,
    the thread seems to relate to some bug in LM5113, the question is if the same bug is in LM5113-Q1 ?
    If not then LM5113-Q1 would seem to be a closer-relative replacement unless there is sth else that speaks nevertheless for LMG1205 ?

    Regards, Pawel
  • In reply to Pawel Piwowarski87949:

    Hi Pawel,

    Yes, this bug also exists in LM5113-Q1. It was fixed in LMG1205, that's why we prefer customers switch to it if possible.

    Best regards,

    Don Dapkus

    Gate Driver Applications Engineering Manager

    Dallas, TX USA

  • In reply to Don Dapkus:

    Hi Pawel,

    do you require Q1 half bridge driver?
    what is your application?
    1205 has improved performance - however similar performance can be achieved with 5113-Q1 if simple workarounds for the bugs are implemented with some external components and applying VDD before VIN. let me know if this is something your interested in going over.

    Thanks,

    Jeff

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.