This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TPS24751: Use of R/C on output for high In-rush current load.

Intellectual 300 points

Replies: 12

Views: 461

Part Number: TPS24751

I am trying to power a large LCD 12V/8A(nom) LCD display from the output of the TPS24751 circuit.

The LCD can have as much as 26A in-rush current when the backlight powers up.

This is over an approximate 3ms period.

Would it be prudent/advisable to change/set the Dv/Dt rise-time on the output by adding the RC to the Gate control output pin of the TPS24751?

If so, what values would you recommend?

Thanks in advance.

  • In reply to Clayton Whitehead:

    Hi Clayton,

    Just a reminder for the test waveforms to close this.

    Best Regards,
    Rakesh

    --------------------------------------------------------------------------------------------------------

    To find the latest information on Power Switches, Visit www.ti.com/powerswitch 

  • In reply to Rakesh:

    Hi Rakesh,

    Thanks for the continued interest.
    Thankfully, we have resolved our issues with the inrush settings and now all is working correctly.
    Thanks for your support and advice.

    Regards,
    Clayton

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.