This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TPS61021A: TPS61021A

Expert 1075 points

Replies: 3

Views: 82

Part Number: TPS61021A

Dear TI Sir

Below  is TPS61021A/TLV61021 block diagram.

I would like to know  V? I?  of  TPS61021A/TLV61021

  • Dear Sir,

    Do you mean the output current, output voltage? I can't understand what your mean?

    Best Regards,
    Helen

    Boost DC/DC Solution

  • In reply to Helen chen:

    The V and I come from Loading

  • In reply to Terry Tseng:

    Dear Sir,

    If you mean it is the voltage and the current from the load, then the maximum external added voltage can be as high as 4.6V, but suggest leave some margin, so 4.2V should be OK. For the reverse current from the load side, actually, once there's reverse current, the high side FET will shut down.

    Best Regards,
    Helen

    Boost DC/DC Solution

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.