This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

BQ24616: BQ24616 charging problem

Expert 3185 points

Replies: 3

Views: 173

Part Number: BQ24616

Dear team,

The current debugging from 1cell-5cell is normal, and the charging current is in line with the design requirements, but when the battery is adjusted to 6cell, as long as a power-on, about 1s time status indicator shows charging, but I did not pick any battery .
Then adjust the resistance and change the original 6cell charge to 5cell charge. The phenomenon is the same as the 6cell charge. What is the problem?

Vin=28V, Iadapter=4A, Iprecharge=0.3A, Icharge=1.5A, charging time is set to 2 hours, when the problem occurs, the input current position is around 0.1A.

Could you please help answer this question?

Thanks & Best Regards,

Sherry

  • Sherry,

    Could you measure the input voltage, PH node and VBAT when the operation is abnormal? Do you use 6 cell battery or battery simulator in the circuit? You commented "I did not pick any battery", but I am not sure what you meant.

    Regards,

    Eric

    Texas Instruments

    Battery Charger Solutions

  • In reply to ezhao:

    Hi Eric,

    I will measure that. Sorry I didn’t express it clearly. I mean I did not connect any battery.

    Best Regards,
    Sherry
  • In reply to Sherry Liang:

    Hi,

    We haven’t heard back from you for a while, the thread is considered solved and closed.

    Thanks!
    Please click "This Resolved my issue" button if this post answer your question.

    Please click "This resolved my issue" button if this post answers your question.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.