This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

UCC28180: AC24V Input U

Prodigy 200 points

Replies: 5

Views: 150

Part Number: UCC28180

Hi Sir:

   We have one application for UCC28180  Which Input is AC24V  and Output is 60V 2A,

We use  Tina II for simulation but output ripple was very bigger ,as attached file(UCC28180-P.TSC) ,would U  please  review it and give us good suggestion.

Thanks

Gorden

.UCC28180-P.TSC

  • Hello Gorden,
    Please use the Excel calculator tool for this application.
    The UCC28180 will work in this application but your TINA results arte not accurate.
    Regards
    John
  • In reply to John Griffin1:

    HI John:

      On the datasheet application schematic ISENSE Pin have one Clamp diode ,what's of parts specification that U recommended?

    Thanks

    Gorden

  • In reply to gorden tsai:

    Hi Gorden,
    You may use a BAT54 small signal diode here
    Regards
    John
  • In reply to John Griffin1:

    Hi John:

      1.Our application input AC24V ,output 60V 100W ,

    2.We are use Excel calculator and modify EVM board some of  component value (ICOMP,VCOMP) base on calculator result .

    3.When loading 100mA seem OK ,but increase loading to 300mA will cause UCC28180 not working ,output voltage equal to input voltage

    Would U help check our Excel file contain correct or not

    Thanks

    GordenUCC28180_12-23.xls

  • In reply to gorden tsai:

    Hi Gordon,
    This post is closed and I am unable to reply.
    Please open a new post with this issue and some one will reply .
    Thanks
    John

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.