This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

WEBENCH® Tools/LMR33630: LMR33630

Prodigy 670 points

Replies: 4

Views: 1835

Part Number: LMR33630

Tool/software: WEBENCH® Design Tools

When I try to simulate Webench tells me it cannot create a design for this device.

Also, Webench will not even start with firefox. Is windows explorer the only browser supported?

Regards,

Kevin

  • Kevin,

    Chrome and Internet Explorer work for me.

    What specs are you trying to design for?

    -Sam
  • In reply to Samuel Jaffe:

    Are you saying webench design for LM33630 works for you?

    Vin is 24V, Iout 3A, I've four designs for Vouts' of 1.21, 1.8, 3.3 and 12V. I'm using the default temp.

    -Kevin
  • In reply to Kevin Lowderman:

    Kevin,

    I was able to create all 4 of your designs in WEBENCH using Chrome with no issue. Please send screenshots of the specs you enter and the error message you get.

    Thanks,
    -Sam
  • Hi Kevin,

    start webbench. Then click onto the dark lower half of screen. After that click onto the control box to allow "Adobe Flash" in Firefox.

    Kai

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.