This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TPS63036: Input Voltage Range

Prodigy 100 points

Replies: 2

Views: 77

Part Number: TPS63036

Hello,

I want to use TPS63036 Buck Boost Convertor for converting 3-6 V Input range to 5 V output. I am using two 3 V coin cells in series as Vtg source.

Is it OK if 6 V input is given as input to the convertor, its range is given as 1.8 V to 5.5 V, but absolute maximum input voltage is 7 V.

Will this configuration be stable.

If not please suggest similar part.

Thanks,

Ameya

  • Hello Ameya,

    maximum operating conditions are stress ratings only, and functional operation of the device at these or any other conditions beyond those indicated under Recommended Operating Conditions is not implied. Also, exposure to absolute-maximum-rated conditions for extended periods may affect device reliability.

    Please have a look at TPS63060.

    regards,
    Julian

    For more information on buck-boost devices have a look at ti.com/buckboost.

  • Hi Ameya,

    We haven’t heard back so we're assuming this answers your question. If not, just post a reply below, or create a new thread if the thread has locked due to time-out.

    Thanks and regards,
    Milos

    ti.com/buckboost

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.