This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

LMZ21701: No 3.3V voltage regulation

Prodigy 20 points

Replies: 3

Views: 65

Part Number: LMZ21701

My application needs to step down 12V to 3.3V. I used LMZ21701 for its compact footprint. My schematic:

But output voltage is not 3.3V, instead it appears to track input voltage, Vout = Vin - 2.1V. At 12V input, I see 9.9V at Vout. How do I achieve correct voltage regulation?

Thanks!

  • Gowtham,

    Your schematic did not post.  Can you re-try?

    Best  Regards,

    John Tucker

    BSR-MV DC/DC Applications

     

    “Working on an automotive power design? Read the E2E technical article Meet European Commission ADAS requirements with TI DC/DC for device recommendations and other helpful resources.”

     

  • In reply to JohnTucker:

    Oops! I hope it shows up this time.

  • In reply to Gowtham M:

    Gowtham,

    Either the module is damaged or the FB resistors are not soldered correctly.  Please check them.

    Best  Regards,

    John Tucker

    BSR-MV DC/DC Applications

     

    “Working on an automotive power design? Read the E2E technical article Meet European Commission ADAS requirements with TI DC/DC for device recommendations and other helpful resources.”

     

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.