• Resolved

TPS51362: MODE pin only one selection

Expert 4005 points

Replies: 1

Views: 21

Part Number: TPS51362

Hello expert,

Customer want to know why there is only one selection for MODE pin which is floating. Since the description in datasheet mention we can set operation frequency through MODE pin but there is only one selection could use. And also, MODE pin is connected to GND in electrical table. Thanks a lot!!

Best regards,

Ann Lien

  • For 51362, Frequency only supports 800K Hz

    For 51363 and 51367, Frequency can support 800K(mode floating) and 400K(mode to GND).

    The table is right.

    Yuchang