Other Parts Discussed in Thread: TIDA-00443
Hello
Please could you give me some explanation (application note or something like that) on how the Vcomp and Icomp are generated inside UCC28180. This is for my personnal understanding :-). In the datasheet, the voltage error amplifier transconductance gain is specified -56µS, that is to say that if V sense is lower than 5V internal regerence, the voltage error output will decrease ???? so Vcomp will decrease and this is not logical... Please could you explain me how it works
I have designed a 2.5 kW PFC for 230Vac mains following the SLUC506revA design calculator. The PFC is fine till 2kW. and from that point I got a big distorsion on the PFC coil current
Yellow is input voltage and Green is PFC coil current for 2.5kW out.
The coil inductance is 200µH for 15A, and is not saturating and variations of compensation components on Vcomp and Icomp had not effect.
In order to solve the problem, I had to reduce Rsense from 0.01 Ohm to 0.006 Ohm and I got a correct shape for inductor current.
Why did I get the wrong shape when Rsense is 0.01 Ohm (although it correspond to the design calculator)
Thank you for your help
Didier