Dear TI power-team,
Regarding BQ25600C, please help clarify the following questions:
1) When used with <= 800mAh batteries, the preference will be to have the charger disabled. Reason being that default charge current would be to high.
- Is it possible to hard-disable it by using the CE pin and then override via i2c !?
- As CE is active low (which is a bit unfortunate as we don't have any valid rails to pull it up to) what is your suggested workaround here?
2) Regarding Type-C and OVP protection, i.e. 20V and surge.
- Would the built in OVP be sufficient (even though 20V is in the absolute maximum range)?
- If not, please suggest a solution for OVP & surge protection while still allowing bidirectional power via OTG
3) As we're planning to use OTG in Type-C DRP modes, can you please supply additional block-diagrams on how this would be implemented.
- It's not clear from the datasheet how the reverse OTG boost -> FET & discharge during disable is working. Please helt clarify.
4) In our case, we need to limit the current to 100-150mA,
- Please propose another pin than "VBUS" (to tap the 5V boosted supply from)
Best regards
David