This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV70012-Q1: TLV70015DSE

Part Number: TLV70012-Q1

Hi,

I've found an issue whereby when a TLV70015DSE regulator is used to supply an op amp mid rail bias the reference 1.5V output is not stable and gradually rises to reach a voltage of approximately 2.18V.

 

On further investigation I found that op amps draw about 0.7uA but believe that the current is sourced from the op amp Vcc via the op amp long tail pair (Vcc= approx 3.0V) that seems to cause the regulator to voltage rise.

 

To try to prove this I replicated the op amp and replaced with a high value resistor of 2M2 to simulate a similar current.  When this resistor was connected to the Vcc rail a similar effect with a rising voltage could be seen.

Note that the same 3.0V rail supplies the input of the TLV70015DSE regulator.

I found that the voltage could be made to return to the correct regulated voltage by connecting a 100k resistor from the 1.5V ref to ground.  My thinking behind this was to provide a return current via ground to the regulator.

 

I would like some help to understand why this is happening as would assume that a regulator would be able to provide a solid voltage source o/p.

As far as I can see the regulator is connected as per recommended in the data sheet and with the recommended decoupling on I/P and O/P of 1uF ceramic capacitor.  An outline schematic  and circuit of the bal to unbal circuit are attached.

 

Thanks

 

Chris