This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40170: Using Faster FETs results in gate drive oscillations.

Part Number: TPS40170

Hello,

I have a question reguarding the ringing issue and the first ringing spike solution with snubber circuits,

when i am using the component for high voltage buck converting (around 35-50 volts input, and 7-8 volts output) what should be the optimal design solution for the ringing issue?

what is the recommanded Cin and Cout in this kind of circuit?

what is the recommanded design for the required voltage output of 7.5v / 6A?