This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27441-G1: pls help recommend a power solution..

Part Number: BQ27441-G1
Other Parts Discussed in Thread: BQ25895, BQ25606, BQ25600, BQ25601

we are designing a system with an battery and dc power supply, the dc-power in is 5V, battery is one cell need charge.  the power rail on board is 3.3v@850mA,  5v@2A, 1.8V@50mA;

if DC-IN exist, the power should come from DC-IN, after remove DC-IN, the power is from battery. could you help recommend a solution?