Other Parts Discussed in Thread: GPCCHEM, BQ34Z100, EV2400
Hello there,
I have a question regarding this one:
In that thread we have obtained help in configuring the BQ34Z100-G1 device to work with 2S lead acid cells 5000 mAh each. Now we need to use the same config, but the cells are replaced with a bigger ones - 8000 mAh. I have loaded the old config and changed:
- Design capacity from 5000 to 8000,
- Design energy from 10000 to 16000.
Then I have charged the battery to full. The problem is that the design capacity remains 4730 mAh (see bellow screenshot). Now I am discharging the cells through a 10 ohm resistor.
I have also attached the gg.csv file. What am I doing wrong here?enersys_e.gg.rar
I would appreciate all help regarding this problem.