This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5145: Question about LM5145 and LM5175 Synchronous operation.

Part Number: LM5145
Other Parts Discussed in Thread: LM5175, , LM5175-Q1

Dear support member,

My customer used LM5145 and LM5175 Synchronous operation.


I hava a question.

I attached question file.
Could you check attached file?


Question
Q1
Could you teach MAX value or Vsynco vs Isyncout characteristic data desired?


Q2
Could you teach Pulse width or duty min / max data desired?


Q3
About the maximum applied voltage recommended value (Is it max 3.3 V?)


Q4
Is there a problem with the connection method?
(Partial pressure resistance constant is provisional value)

Best regard.
Bob Lee.LM5145 and LM5175_question.pdf