This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TPS53014: TPS53014 question about Is it damage the IC when the input / output voltage reverses?

Genius 5540 points

Replies: 2

Views: 87

Part Number: TPS53014

Dear supportmember

My customer used TPS53014.

I have a question.

(Situation)
First
TPS53014 turns the output low by setting EN low.

Second
The input voltage is lowered.

When input voltage is lowered,the voltage of the output of TPS53014 remains.
The input / output voltage reverses by about 600 mV max.


(Question)
There was a situation to reverses by about 600 mV,
Is there any possibility that this will damage the IC?


Best regard.
Bob Lee.

  • Bob,

    The condition you described is okay.

    Regards,
    Mathew
  • In reply to Mathew Jacob1:

    Dear Mathew,

    Thank you very much for reply.

    I reply my cusotomer your answer.
    I will feed back it.

    Best regard.
    Bob Lee.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.