Other Parts Discussed in Thread: LP8758-B0
Hi,
It is a question about the change from Rev. A to Rev. B.
Q1.About changing recommended operating range
In the LP8758-E0, there is a part changed to "VANA with 3.6 V maximum".
In LP 8758-B0, there is a part changed to "VANA up to 3.6".
Are these meanings the same?
Q2.About 7.3.2 Power-Up
I think that it is necessary to wait 1.2 ms until I2C host R / W after setting NRST high.
It is 700 μs at RevA, will it be listed in Revision History?
PCN of LP8758-B0 was the same change, but B 0 is listed in Revision History
Best regards,
Yuto Sakai.