This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 494
Part Number: TPS65381A-Q1
Is there a power estimator for the TPS65381A-Q1?
Best Regards,
Scott Monroe
--------------------------------------------------
For more information on Multi-Channel Power Management ICs:
Find the right power solution for your processor or FPGA. Visit www.ti.com/SoCPower today!
Yes, attached find a power estimator spreadsheet.
TPS65381A-Q1 Power Estimator - E2E FAQ.xlsx
The user can input the supply voltage (VBAT), the configuration voltages for VDD3/5, VDD1 and VSOUT1, the supply source for VSOUT1 (VDD6 or VBATP), load currents for the regulators, Vf of the diode, DCR of the inductor. As the user enters these inputs into the yellow cells with blue font the power estimated for the device and in external components (diode, VDD1 FET and inductor) will be calculated.