Other Parts Discussed in Thread: TPS63001, TPS63031, , TPS63805, LP2985
Hi!
I'm working on a project with a lipo battery. The battery works in a range of 2.9 to 4.2 V, but the system should be feed with 3.3 V.
From my search, I found that the component that best suits my issue is a buck-boost converter. Since the output voltage must be 3.3 V and the current is 40 - 60 mA, what component do you think is best for my project, TPS63051, TPS63001 or TPS63031. I'm focus on high efficiency rather than cost or size. I've read all the literature but I can't understand which one is better for my needs.
Thank you.