Hello, I'm trying to find out if there is a way I can enable the PACK+ output on the BQ4050 without tying in a "wake" button or FET_EN command, or similar physical button to it, so it will turn on as soon as the battery is connected. I have tried to set the wake voltage as low as possible, enabled FET_EN via Manufacturer Access, among many other settings. Is there a list of options I can program on the firmware that would enable this to always be on? I am hoping I can do this so I don't have to redesign my board (that doesn't have a wake button), with a special circuit that only temporarily fires a short to PACK+ when a battery is connected.