Other Parts Discussed in Thread: TPS61023, , , TPS61022
Vout is not regulating to design parameters unless the Rload is removed and reattached or wiggled.
Rload varies from 1.6Ohms to 2.6Ohms depending on make and model of the external Vape Cartridge Atomizer
Vout is set to 4.2V
My schematic and physical board design followed the datasheet and Webench constraints.
The design includes a microcontroller to control the EN pin of the TPS61230 device when a user asserts an external button/switch. When the but/swtch is pressed the microcontroller asserts the EN pin and the TPS61230 powers the Atomizer. At the initial power on state (EN Asserted) the Vout never exceeds 1.28Volts and remains at this level as long as the button is asserted. Once the button is no longer pressed the EN pin is taken to a low level and Vout goes to 0.0V, TPS61230 disabled.
During the initial power on state and while Vout is at 1.28V; if Rload is disconnected and then reconnected Vout will rise to the design Vout of 4.2V. Wiggling Rload will accomplish the same results.