Hi :
I am using TPS92602 boot topology to drive 15 LEDs. Because one of my PCBA board can not achive my lux requirement so I analyze this board and found something strange.
Figure 1 is good board GDRV2 waveform,Figure 2 is bad board GDRV2 waveform ,duty time is very different. This different duty time cause different LED current. Figure 3 is good board LED current when PWM dimming and Figure 4 is bad board LED current. Bad board LED current peak is higher but time is narrow. When I increase PWM dimming duty, the peak current value will decrease but good board peak current change a little when I increase PWM dimming duty. I want to all my boards behavior like Figure1.
ICTRL2 voltage is 32.7mV
DC/DC PWM frequency is 600KHz external
PWM dimming frequency is 2KHz
PWM dimming duty in below figure is 1/200.
Vin is 19V
Figure 1
Figure 2
Figure 3
Figure 4
Figure 5 schematic