Hi
The customer would like to reduce the components around TPS610981.
And we have two question.
1)Our customer are considering such as a following configuration.
Can we remove the diode at the output(VMAIN) line?
We are considering the case of no BAT or no-battery voltage.
If VIN is 0V, VMAIN is 5V and may cause by the reverse current flow from VMAIN to VSW via the body diode of FET.
Is my understanding correct? If it so,we can not remove the diode.
2)The customer would like to consider to reducing the current consumption of system around TPS610981.
What is the components can we reduce the current consumption? L or Rin will be impact to the current consumption?
Best Regards,
Koji Hamamoto