According to the accessory, when the power supply is used, the current will rise slowly, and the power supply will enter the current protection mode.
VDD = DC 5V , V33 = DC 3.3V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
According to the accessory, when the power supply is used, the current will rise slowly, and the power supply will enter the current protection mode.
VDD = DC 5V , V33 = DC 3.3V
Dan,
Please provide the full orderable part number so that I can verify that you have the device configured properly for the OTP you are using.
Regardless of OTP, there are a few issues with the connections in this schematic:
1. RESET_OUT should not be grounded. This is a push-pull output that goes high when the device is finished turning on. Shorting to ground is not advised.
2. INT should be left floating if not using it (though you will not be able to see if an interrupt is generated)
3. LDOVANA_OUT, LDOVRTC_OUT, VCCA, and SMPSx_IN require capacitors (see recommended values in datasheet)
4. SYNCCLKOUT should be left floating if you are not using it
Please see the schematic checklist for how to handle each pin: www.ti.com/.../slvae13
Thanks,
Nastasha