Other Parts Discussed in Thread: MULTIPKGLDOEVM-823
Hi team
customer wants Vout = 5.7V at Max Iout 80mA with Vout deviation = +- 3.5%.
he will use TPS76301-Q1 for adjustable Vout.
D/S says Vout deviation = +- 3% for 5V <= Vout <= 1.5V at 100mA for entire temperature range as below.
My question is D/S also can ensure +- 3% for Vout = 5.7V at 100mA for entire temperature range ?