Dear all,
Couold you teach the meaning of absolute max of MAX of Vout 'min(VIN + 0.3, 20)'?
My understanding is below,
> We need use the smaller value which 'VIN+0.3' or '20' dependingon the conditions.
> If VIN = 20V, this MAX rating is just 20V.
> If VIN = 10V, this MAX rating is 10.3V (10+0.3V).
> In detail, If VIN = 19.9, this MAX rating is 20V (not 20.2V).
Is my understanding correct?
Best regards,