Part Number: BQ27GDK000EVM
Hi,
I am checking all the configuration parameters for this EVM in order to see how they match my battery. The specs of the battery are 550 mAh and 4.2 V; according to the vendor, it needs to be charged at 0.5C (275 mA) and Taper current to be 0.05C (27 mA). Therefore, I would need to set this in BQStudio to fully charge the battery. As this is not mentioned in the User Guide, I looked at the datasheet of the BQ24192 and the minmum taper current could be 128 mAh.
Am I missing something or is it that I am not going to be able to use the GDK to automate the charge and discharge cycles?