I am trying to power a large LCD 12V/8A(nom) LCD display from the output of the TPS24751 circuit.
The LCD can have as much as 26A in-rush current when the backlight powers up.
This is over an approximate 3ms period.
Would it be prudent/advisable to change/set the Dv/Dt rise-time on the output by adding the RC to the Gate control output pin of the TPS24751?
If so, what values would you recommend?
Thanks in advance.