What is the frequency tolerance in CCM mode?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Elder,
Please refer figure 17~20 in datasheet. It shows the frequency with load regulation.
Best Regards,
Edwin.
Hello, Edwin.
The information is meant to the specification of the design and will be verified. I need to have a tolerance to be able to verify if the design is still within acceptable tolerances and, therefore, OK.
Hi Elder,
I have asked the test engineer who write the TPS568215 test program. He maybe can provide the tolerance value. Once I got the result, I'll tell you. It takes 1 or 2 days. Please wait in patience.
Best regards,
Edwin.
Hi Elder,
For a given Vin/Vout, Tolerance is +/-10% depending on its typical frequency. For example: Vin=12V and Vout=1.2V, the typical frequency would be ~400kHz. Min is 360 kHz and max is 440 kHz.
Best Regards,
Edwin.
Hello, Edwin.
That provides the ballpark I need for my specification.
Thank you very much.
Elder.