Hello,
i uploaded a File to ttps://www.ti.com/powercalculator/docs/gpc/gpcUpload.tsps . Usually it takes around 5-10 Minutes to get an answer. I am at 2h right now and this is highly unusal at least in my experience. I know it tells me that the report will be sent "approximately one hour" after and is not guaranteed but I still reuploaded the Data 1h later after i checked with our IT that nothing changed with the E-Mailfilters (*.zip Attachment).
Are there some Problems with the service ? I don't mind having to wait when i know it is in the works but other than the reply i can't see if there is some kind of error in my uploaded Data. To start the golden Cycle i was hoping to get the ChemID soon.
thanks in advance
Robert