This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR23625: feedforward capacitor

Part Number: LMR23625

Hi team,

Our customer is designing circuits using LMR23625.

They are concerned about the need for feedforward capacitors and constant design.

#1

How can we decide whether this is necessary?

They want to reduce the number of parts, so I do not want to implement Cff unless necessary.

#2

If necessary they will decide Cff according to the following formula in the data sheet.

Rfbt is 12kohms and Cout is 44uF.

Cff is calculated as 175pF.

I tried to check with webench, but I can not check the Bode plot because the capacity value is not recommended and I can not input it.

Could you check whether this constant is okay?

Best regards,

Tomoaki Yoshida