This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Normally ON powerFET

Prodigy 20 points

Replies: 1

Views: 74

I need a normally ON power switch. High-ish voltage (200V) and current (50A total with parallel devices), and low ON resistance are main requirements. Seems that only IXYS makes any depletion mode power MOSFETs and they are very pricey. I understand GaN devices are inherently normally ON, but it appears the GaN parts from TI and others are using a cascode FET on all their devices to make them function as normally OFF devices for use in the typical power switching circuit. But, the datasheets don't exactly call this out, nor do the search tools and I got tired of looking. Does TI have any parts that meet this requirement or any plans for any? Or, do you know of any others besides IXYS?

  • Hello Kurt,

    Thanks for your interest. 

    TI GaN is a depletion mode device, but it does not work in cascode manner. We have an internal buck-boost converter to generate a negative voltage, which directly drives GaN devices without switching the Si part. Currently, there is no plan to release the normally-on depletion mode device separately. The whole device will be a power stage which would act like normally-off. 

    Thanks and regards,

    Lixing

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.