This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 7
Views: 152
Part Number: TPS65084
Hi Sir,
Our customer use the TPS650842 for Intel Braswell Platform.
But they are found out system in sleep or shut down SWB2 have 1V ~1.8V level,
The SLP_S3 status is Low.
Could you please get me some suggest for this issue?
Hugo
Our customer need add the discharge on schematic.
In reply to Hugo Liu:
Thank you, Nick Jakse--------------------------------------------------Find the right power solution for your processor or FPGA. Visit www.ti.com/SoCPower today!
In reply to Nick Jakse49:
Hi Nick,
May I double check with you, So try to setting 100 or 200 or can be improve this issue?