Other Parts Discussed in Thread: TLV61046A, TPS61046, LMR36006, LMR36006-Q1, TPS2595, LMR36015
My current system has 5V available and I need to provide 10V to an external device. It is OK if this external voltage is not referenced to GND, and given some size and cost constraints, I think the smallest solution it to use an inverter (like the LM2776) and provide +5 and -5 to the external device, who should be happy to see 10V (let me know if this is incorrect).
Assuming that this is a valid way to provide a 10V output, my concern is how to protect the LM2776 from ESD, or any other normal concerns related to an external connection. For example on the +5V side I can use a diode to prevent reverse voltage, but on the -5V side that diode would need the opposite polarity, which would not help if a positive voltage is accidentally applied to that pin.
Perhaps there is an application note available that would help with this?