My application may see currents in excess of 150A. A current sense resistor is just not practical. I intend to use an Allegro hall effect device and scale the output to the SRN input range; SRP tied to stack '-'. The current consumption of this device (15mA max) is not insignificant. While the BQ34Z100-G1 is in sleep mode I will power down the Allegro device to optimize battery consumption. The standard 'Alert' options (7.3.14 Table22, DS July2016) do not offer an "awake" output. The last sentence of the paragraph under Table21
"See the reference schematic (Figure 17) for filter implementation details if host alert sensing requires a continuous signal."
implies that pin TS/P6 should be used for this function. ("Host Alert" not to be confused with "Alert".) Monitoring pin11 on my EVM, while the 'G1' is in sleep mode (no I2C activity), I see a 140ms width pulse every 20s. This is consistent with biasing the external thermistor prior to reading. I intend to use this signal to gate power and enable biasing of the Allegro device. The 'G1' datasheet does not give any timing information relative to this signal and internal operations. The 'G1' datasheet does mention a 1s "typical" acquisition time (6.10, 'tSR_CONV'). This appears to be four times longer than expected for the same bit resolution relative to (6.11, 'tADC_CONV').
What is timing relationship of the TS/P6 activity to V(SRN) and V(SRP) conversion?
When are the inputs sampled?
Do the inputs need to be stable for the entire conversion period?
Thank you,
Noel Lanier