My customer is using TPS61169 to light up 8s series, 2 parallel total 16 LEDs. Input voltage is 4V not 5V shown in the picture below.
The schematic is as below.
At lowest duty cycle of 1%, the waveform is as below:
At brightest dimming, the waveform is as below:
They also measured the input current with multimeter. They've already limited the output current to 40mA. So with input current =450mA, the output current should be 450mA*4V*efficiency/22.5=80mA if efficiency=100%. which is far bigger than limited.
It seems that the problem is at the abnormal current waveform, so could you please tell what may cause this abnormal?
darkest dimming VIN current |
brightest dimming VIN current |
|
32mA |
450mA |