Good evening to everyone,
My name is Dario Laezza and I'm an electronic engineering student, with other collegues we are designing a Pre-charge circuit with the IC in the thread's title. Because of the capacitive load (300uF) we have chosen a quite big Bootstrap capacitor (20uF). In order to complete the charge and loose at maximum the 10% of the charge on the Boot capacitor we must modify the 10k resistor placed on the gate of the both switches in the application note. We have read that this resistor is used to avoid a non intentional driving when the IC is not well soldered. My question is: is there any problem if we use a 100k resistor instead of 10k? This help us to loose less charge as possible. Thank you to everyone and good evening.
Best regards
Dario Laezza