Other Parts Discussed in Thread: GPCCHEM, EV2400
Hi
case: Lead Acid battery 36V 9000mAhr; 2438.logs.zip
Cell term voltage 1.6x18 = 28.4V
The hardware of my board misses the filter at the current input. R sens : 0.01E
Discharge @2A: OK
Discharge @4A: at Remcap exactly 8000mAhr : SOC 90->0% , Full ChargeCap 9000->1001 . The same happens with a constant Voltage instead of the battery.
It happens with all my boards.
Must be some setting?
When recharging the battery the Remcap goes from 0-> 1001, then steps to 9000.
Log from Bq studio:
Sample | DateTime | ElapsedTime | Control | CtrlStatus | StateofCharge | MaxError | RemCap | FullChgCap | Voltage | Current | AvgCurrent | Temperature | AverageTimeToEmpty | AverageTimeToFull | AvailableEnergy | AveragePower | InternalTemperature | CycleCnt | StateofHealth | ChargeVoltage | ChargeCurrent | PackConfig | Flags | Flags B | GridNumber | LearnedStatus | DoDatEOC | Qstart | TrueRC | TrueFCC | StateTime | DOD0PassedQ | DOD0Time | DOD0 | QmaxDOD0 | QmaxPassedQ | QmaxTime | LogRowTime(ms) | LogStatus |
1 | 2018-12-19 11:03:49 | 4034 | 0x0203 | 0x0203 | 100 | 100 | 8979 | 9000 | 42534 | -4180 | -2966 | 25.6 | 182 | 65535 | 17685 | -9877 | 27.3 | 0 | 100 | 43200 | 4500 | 0x09D9 | 0x1291 | 0x0400 | 1 | 4 | 0 | 0 | 8977 | 9000 | 45 | 23 | 0 | 0 | 0 | 23 | 0 | 886 | SUCCESS |
135 | 2018-12-19 11:12:45 | 540091 | 0x0203 | 0x0203 | 93 | 100 | 8358 | 9000 | 42552 | -4165 | -4167 | 27.0 | 120 | 65535 | 17538 | -9846 | 28.5 | 0 | 100 | 43200 | 4500 | 0x09D9 | 0x1191 | 0x0400 | 1 | 4 | 0 | 0 | 8357 | 9000 | 579 | 643 | 3 | 0 | 0 | 643 | 3 | 887 | SUCCESS |
182 | 2018-12-19 11:15:53 | 728112 | 0x0203 | 0x0203 | 91 | 100 | 8142 | 9000 | 42552 | -4164 | -4164 | 27.1 | 117 | 65535 | 17487 | -9844 | 28.6 | 0 | 100 | 43200 | 4500 | 0x09D9 | 0x1191 | 0x0400 | 1 | 4 | 0 | 0 | 8141 | 9000 | 766 | 859 | 4 | 0 | 0 | 859 | 4 | 887 | SUCCESS |
210 | 2018-12-19 11:17:45 | 840125 | 0x0203 | 0x0203 | 90 | 100 | 8013 | 9000 | 42552 | -4162 | -4162 | 27.2 | 116 | 65535 | 17456 | -9837 | 28.7 | 0 | 100 | 43200 | 4500 | 0x09D9 | 0x1191 | 0x0400 | 1 | 4 | 0 | 0 | 8012 | 9000 | 878 | 988 | 4 | 0 | 0 | 988 | 4 | 887 | SUCCESS |
211 | 2018-12-19 11:17:49 | 844118 | 0x0203 | 0x0203 | 89 | 100 | 8009 | 9000 | 42552 | -4162 | -4162 | 27.1 | 115 | 65535 | 17455 | -9839 | 28.7 | 0 | 100 | 43200 | 4500 | 0x09D9 | 0x1191 | 0x0400 | 1 | 4 | 0 | 0 | 8007 | 9000 | 882 | 993 | 4 | 0 | 0 | 993 | 4 | 888 | SUCCESS |
212 | 2018-12-19 11:17:53 | 848128 | 0x0203 | 0x0203 | 89 | 100 | 8004 | 9000 | 42552 | -4162 | -4162 | 27.2 | 115 | 65535 | 17454 | -9839 | 28.7 | 0 | 100 | 43200 | 4500 | 0x09D9 | 0x1191 | 0x0400 | 1 | 4 | 0 | 0 | 8002 | 9000 | 886 | 998 | 4 | 0 | 0 | 998 | 4 | 888 | SUCCESS |
213 | 2018-12-19 11:17:57 | 852122 | 0x0203 | 0x0203 | 89 | 100 | 7999 | 9000 | 42552 | -4162 | -4162 | 27.2 | 115 | 65535 | 17453 | -9839 | 28.7 | 0 | 100 | 43200 | 4500 | 0x09D9 | 0x1197 | 0x8400 | 2 | 4 | 0 | 0 | -1 | 1001 | 890 | 1002 | 4 | 0 | 0 | 1002 | 4 | 887 | SUCCESS |
214 | 2018-12-19 11:18:01 | 856133 | 0x0203 | 0x0203 | 0 | 100 | 0 | 1001 | 42552 | -4163 | -4162 | 27.2 | 0 | 65535 | 0 | -9841 | 28.7 | 0 | 100 | 43200 | 4500 | 0x09D9 | 0x1197 | 0x0400 | 2 | 4 | 0 | 0 | -6 | 1001 | 894 | 1007 | 4 | 0 | 0 | 1007 | 4 | 886 | SUCCESS |
215 | 2018-12-19 11:18:05 | 860125 | 0x0203 | 0x0203 | 0 | 100 | 0 | 1001 | 42552 | -4163 | -4162 | 27.1 | 0 | 65535 | 0 | -9841 | 28.7 | 0 | 100 | 43200 | 4500 | 0x09D9 | 0x1197 | 0x0400 | 2 | 4 | 0 | 0 | -11 | 1001 | 898 | 1012 | 4 | 0 | 0 | 1012 | 4 | 887 | SUCCESS |
216 | 2018-12-19 11:18:09 | 864135 | 0x0203 | 0x0203 | 0 | 100 | 0 | 1001 | 42552 | -4163 | -4162 | 27.2 | 0 | 65535 | 0 | -9841 | 28.7 | 0 | 100 | 43200 | 4500 | 0x09D9 | 0x1197 | 0x0400 | 2 | 4 | 0 | 0 | -15 | 1001 | 902 | 1016 | 4 | 0 | 0 | 1016 | 4 | 886 | SUCCESS |
settings and log are in included zip
Thanks in advance
Dig