This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

LMZ23608: no load operation

Prodigy 50 points

Replies: 6

Views: 100

Part Number: LMZ23608

Hi!

We have chosen LMZ23608 module for speeding up our design. Input voltage: 11 ... 21V. Output Voltage: 5V. Max output current: 6A. I think it will all work fine. We have only one concern. Our minimum  output current can be as low as 0 (ZERO) Amps. In this respect I am not sure regarding module  control loop stability,  module heating, module internal componets stress, etc.

Also it is difficult to rely on PSPICE models as they were mathematically prepared for the case when RLoad is not infinity.

Did anyone try to use this module at no-load condition? What is the value of minimal load (if any)?

Any help appreciated!

Thank you, Andrei

  • Hello Andrei,

    The LMZ23608 should work fine with no load. I don't foresee any issues.

    Page 10 of the datasheet has line and load regulation curves that start at no load condition.

    Here is a link to the datasheet:

    Let us know if you need any additional support. 

    Cheers, 
    Denislav

  • In reply to Denislav Petkov:

    Dear Denislav,

    Thanks for the quick reply!

    Previously we have tried MIC45212-2 (here is the link to the datasheet ). 

    MIC45212 curves started also at no-load condition. But when we installed it into the board at no load module temperature increased swiftly upto 85C and noizy sound appeared. That is why this time I am very suspicious :)

    Dear Denislav,

    If you have LMZ23608 Evaluation Board at your hands could you please conduct no-load experiment and report module temperature or abnormal behaviour if any? For us this is very important.

    Best Regards

    Andrei

  • In reply to Andrei Chegurov:

    Hi Andrei,
    Let me look for an evaluation board. We can do this test for you. I hope to give you some data on this tomorrow.

    I am confident we won't see an issue but we will take the data for you.

    Cheers,
    Denislav

  • In reply to Denislav Petkov:

    Hello Andrei, 

    Here are some measurements from the evaluation board. 

    21Vin 5Vout No Load:

    12Vin 5Vout No Load:

    These were taken at room temperature. 

    I hope this helps. 

    Cheers, 
    Denislav

  • In reply to Denislav Petkov:

    Dear Denislav,

    Thank you for your time and efforts! We are putting module into design.

    Sincerely Yours
    Andrei
  • In reply to Andrei Chegurov:

    Thank you for utilizing the E2E forum Andrei.
    Cheers,
    Denislav

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.