Other Parts Discussed in Thread: BQ34Z100, BQSTUDIO,
HI team
Would you please support for my questions ?
1.Golden image at production line
* How much time to required to write GG data to device at production line ?
*To write it, should it use by I2C command.
*To write it , is it necessary unseal, after writing, should be set seal.
2.Average current
How much is sampling time ?
3. Max error (Table 4)
*Does “Event” happen by bq34z100 ?
*For ex, When Ra table is updated, Does Qmax change to 5% ?
*When reset happens ?
*After learning, is Max error 1% ?
*After writing golden image, is Max error 1% ?
4,What is a Version of FW and Hard ware?
5.Charge termination
In case of Li-ion cell. How to judge the termination ?
Is it judged by taper current that is stored Data flash ?
6.Manufacturer Information Block
What is this purpose ? Which case customer should use ?
best regards K.Kanao